AXIS#.IL.FF

Description

AXIS#.ILClosed "Instruction List" This is a low-level language and resembles assembly.FF reads the present current loop overall feed-forwardClosed This describes an element or pathway within a control system which passes a controlling signal from a source in the control system's external environment, often a command signal from an external operator, to a load elsewhere in its external environment value. It is the sum of the following feed-forward paths:

AXIS#.IL.FF is calculated using the following variables' values at the time it is called:

AXIS#.IL.FF = AXIS#.IL.KACCFF * Acceleration Command + AXIS#.VL.KVFF * Velocity Command + AXIS#.IL.FRICTION (if motion is currently commanded) + AXIS#.IL.OFFSET (always) + * AXIS#.FBUS.IL.FF (if fieldbus connected)

For EtherCATClosed ***EtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs:

AXIS#.FBUS.IL.FF is the injected current feedforward, which corresponds to Object 60B2h: TorqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist Offset. The scaling for the torqueClosed Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist offset is done with 1/1000 rated torque. In AKD, a value of 1000 means AXIS#.ICONT will be commanded in AXIS#.FBUS.IL.FF (if AXIS#.IL.KBUSFF is set to 1).

AXIS#.IL.KBUSSFF is a gain setting for the feedforward value AXIS#.FBUS.IL.FF. It needs to be set to greater zero to let AXIS#.FBUS.IL.FF take effect. AXIS#.IL.KBUSFF can be accessed by SDO object 50E2h/0.

The AXIS#.FBUS.IL.FF gain can be commanded through EtherCAT in all DS402 operating modes.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

Arms

Range

N/A

Default Value

N/A

Data Type

Float

See Also

AXIS#.IL.KVFF, AXIS#.IL.OFFSET, AXIS#.IL.FRICTION, AXIS#.IL.KACCFF

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Fieldbus Information

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.FF

5804

16AC

Signed32

Read Only

-

AXIS2.IL.FF

71340

116A

Signed32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.FF

5804

Float

Read Only

-

Related Topics

Current Loop